Technical FAQs

Ask a Question

What is a XCLJ176 PG13 limit switch?

The correct part number is XCLJ167. This is a British XCKJ painted red. Customer can order a XCKJ167PG and get what he wants minus the red color. Contacts are A300, Q300 and 10A continuous. The are snap action type contacts in 1 normally open, 1 normally closed arrangement.


CTA-ID : 2048772
Was this helpful?
What can we do to improve the information ?