Technical FAQs

Ask a Question

What is a FA322?<br />

It is an obsolete bus plug. It was a 3P3W 60A 250V fusible unit (floor operated) for the older 100A plug in busway. It can be replaced with a PIN100FA plug-in unit. This device is an enclosure only. The part number for the floor operator attachment is P11FA. The part number for the QO breaker is QO260.



CTA-ID : 2048768
Was this helpful?
What can we do to improve the information ?