Technical FAQs

Ask a Question

What is the replacement main breaker for a QOBW20M100-2 load center?

Issue:
Repair parts

Product Line:
Obsolete QO LC

Cause:
Maintenance

Resolution:
The QOBW20M100-2 is the box reference number, not the load center catalog number. This box was used with the QO12-20M, QO14-20M and QO16-20M load centers. These load centers used the Q12100TF main breaker, which is `Obsolete` with no replacement.



CTA-ID : 2048339
Was this helpful?
What can we do to improve the information ?