Technical FAQs

Ask a Question

What is the voltage rating for a 82345DS double throw safety switch?

This switch is rated 600VAC or 250VDC maximum. The 250VDC rating was incorporated in February, 2009. Devices manufactured before then would not have the 250VDC markings on the wiring diagram label.

CTA-ID : 2048583
Was this helpful?
What can we do to improve the information ?