Technical FAQs

Ask a Question

Is PLA36060 a valid number?

Order as PLA34060. For Powerpact P frame breakers with the L interrupting, it is ordered as a 480V breaker. The breaker is rated up to 600V but at a lower AIC (25 K) than typical ``L`` interrupting ratings.

CTA-ID : 2048300
Was this helpful?
What can we do to improve the information ?