Technical FAQs

Ask a Question

Does Square D offer an enclosed circuit breaker with a keyed interlock factory installed?

Issue:
Product feature

Product Line:
Enclosed Circuit Breaker

Cause:
Selection with special feature

Resolution:
In most cases, yes. Please contact 1-888-778-2733, Option 1, Option 1, Option 4 to determine if an enclosed circuit breaker with a factory installed keyed interlock can be offered. 


CTA-ID : 2048025
Was this helpful?
What can we do to improve the information ?