Technical FAQs

Ask a Question

Can the RM4TU02 be used on a 480V nominal voltage system?

Issue:
Can the RM4TU02 be used on a 480V nominal voltage system?

Product Line:
RM4T Measurement Relays

Environment:
Zelio Control Measurement Relay

Cause:
Application is calling for measuring 480 volts.

Resolution:
No, the nominal voltage range is 430V max.  Suggest using the RM17 or RM35 line instead.
 
Was this helpful?
What can we do to improve the information ?