Technical FAQs

Ask a Question

Are the dimensions the same for a QO120 and a QO120GFI?

No, the dimensions are different. The QO120 is 3.00 inches in height & the QO120GFI is 4.12 inches in height.
Dimensions for the all the QO type breakers can be found in the Digest.

CTA-ID : 2048007
Was this helpful?
What can we do to improve the information ?