Technical FAQs

Ask a Question

Is there a non-fused version of the PQ4203G?<br />

No, non-fusible PQ plug-in units are not available. There are 30 amp circuit breaker plugs available but they do not use the PQ enclosure.


CTA-ID : 2048656
Was this helpful?
What can we do to improve the information ?