Technical FAQs

Ask a Question

Does the Series D Line Isolation Monitor, catalog number IGD, have any field serviceable parts? Can it be returned for repair?

The only field replaceable parts on the Series D Line Isolation Monitor (LIM), catalog number IGD is the 1/4 amp semi-conductor fuse, type TR5 (catalog # TR5), of which there are two in each LIM. Otherwise, there are no field serviceable parts. This device can not be returned for repair.


CTA-ID : 2048648
Was this helpful?
What can we do to improve the information ?