Technical FAQs

Ask a Question

Does Square D offer a double throw safety switch: 100 amp, 3 phase, 240V, fused, in a stainless steel enclosure?

Issue:
Selection

Product Line:
Double Throw Safety Switch

Cause:
Selection

Resolution:
We do not offer in a fusible device. We do offer a 600V, non fusible, 100 ampere, 3 pole switch: Catalog Number DTU363DS.


CTA-ID : 2048702
Was this helpful?
What can we do to improve the information ?