Technical FAQs

Ask a Question

What is the wire range that can be accommadated by the lugs that are provided with the standard I-Line II end cable tap box?

The phases lugs will accomodate 1/0-600 kcmil (mcm) Copper or Aluminum conductors.
The ground lugs will accomodate the following based on the rated amperage for the end tap box:

800 amp - 2000 amp = #6 -300 kcmil (mcm) Copper or Aluminum conductors.
2500 amp - 5000 amp = 2/0-500 kcmil (mcm) Copper or Aluminum conductors.


CTA-ID : 2048486
Was this helpful?
What can we do to improve the information ?