Technical FAQs

Ask a Question

Is a DTU366AWK double throw safety switch provided with a dual cover interlock?

Yes, this switch is supplied with a dual cover interlock. With the switch in either of the ON positions, the cover cannot be opened. There is no defeat mechanism for this feature. With the switch cover open and the switch in the OFF position, the switch cannot be operated to either of the ON positions. There is a defeat mechanism to allow this feature to be overridden.


CTA-ID : 2048566
Was this helpful?
What can we do to improve the information ?