Technical FAQs

Ask a Question

Is a Class 30 trip available on the Motor Logic Overload Relays?<br />

No, only Class 10 or Class 20 trip is available on Motor Logic Solid State Overload Relays. Form H30 is for the feature unit which is selectable for Class 10 or 20.


CTA-ID : 2048460
Was this helpful?
What can we do to improve the information ?