Technical FAQs

Ask a Question

What is the purpose of the two tiny screws, 6-32 x 1/4``, similar to panhead screws, shipped with I-line panels in the hardware bag?

These are for mounting the panelboard nameplate.


CTA-ID : 2048406
Was this helpful?
What can we do to improve the information ?