Technical FAQs

Ask a Question

What is the minimum load (volts and amps) for the M9 OF switch?

It is rated for 24 Vdc and 10 mA. It may work at 12vdc and 20mA, but performance at this level is not certified.


CTA-ID : 2048328
Was this helpful?
What can we do to improve the information ?