Technical FAQs

Ask a Question

Do the padlock attachments for the Powerpact M and P frame breaker lock in the OFF position only?

Yes. Both the removable padlock S44936 and the fixed padlock S32631 lock in the OFF position only.


CTA-ID : 2048528
Was this helpful?
What can we do to improve the information ?