Technical FAQs

Ask a Question

What is the number of operations for a motor operator on a Powerpact breaker?

The UL Standard 489 endurance requirement for an electrical operator is equal to the circuit breaker?s no-load endurance requirement.


CTA-ID : 2047391
Was this helpful?
What can we do to improve the information ?