Technical FAQs

Ask a Question

What are the restrictions to mounting QOB3110VH and larger branch breakers in a NQ panelboard?

Issue: What are the restrictions to mounting QOB3110VH and larger branch breakers in a NQ panelboard? Product Line: Panelboards. Environment: Products sold in the United States. Cause: Product featues. Resolution: The QOB3110VH through QOB3150VH requires 6 vertical spaces and the largest branch breaker which can be mounted adjacent to (across from) it is 20A. CTA-ID : 2047356
Was this helpful?
What can we do to improve the information ?