Technical FAQs

Ask a Question

The MA1000F enclosure is obsolete and no longer available. What enclosure can be used for a MAL or MHL circuit breaker?

The enclosures for the MAL family of circuit breakes are obsolete and no longer available. Consider using a PowerPact M-frame circuit breaker (800A max) or PowerPact P-frame circuit breaker (1200A max). A NEMA 1 flush mount enclosure is not available for the PowerPact M-frame or P-frame breakers. Consider using a NEMA 1 surface mount enclosure. The NEMA 1 surface mount enclosure for the M-frame PowerPact would be M800S. The NEMA 1 surface mount enclosure for the P-frame PowerPact would be P1200S.


CTA-ID : 2047249
Was this helpful?
What can we do to improve the information ?