Technical FAQs

Ask a Question

Are there optional lugs available for the NSJ breaker that will accept (2) wires or cables?

Catalog number 32510 contains lugs and hardware for one side of breaker that will accommodate (2) 2/0 - 350 kcmil Cu and (2) 2/0 - 500 mcm Al.


CTA-ID : 2047463
Was this helpful?
What can we do to improve the information ?