Technical FAQs

Ask a Question

What is the required enclosure size for the 100% rated Compact NSJ and Powerpact D circuit breakers?

100% rated: suitable for continuous operation at 100 percent of rating only if used in a minimum cubicle space of H40 by W14 by D4 inches without ventilation.
Note: 100% ratings only apply to 400 amp frame and smaller. The 600 amp frame is 80% rated.

CTA-ID : 2047414
Was this helpful?
What can we do to improve the information ?