Technical FAQs

Ask a Question

Can the rating plug on the EZM main circuit breaker catalog number EZM31200CBU be changed to create a EZM31600CBU?

Issue:
Product Design features

Product Line:
EZM Metering

Environment
Maximum Mains rating

Cause:
Application

Resolution:

No. The 1200A unit is UL listed and labeled as 1200A maximum device and cannot be changed to a higher amperage.


CTA-ID : 2047570
Was this helpful?
What can we do to improve the information ?