Technical FAQs

Ask a Question

What is the maximum number of 9999WX11 auxiliary contacts that may be mounted to a 8502WGO3?

A maximum of four additional auxiliary contact units may be installed on each non-reversing contactor.


CTA-ID : 2047173
Was this helpful?
What can we do to improve the information ?