Technical FAQs

Ask a Question

What does the suffix -1677 mean in part number KA362251677?

Suffix 1677 includes 2A/2B auxiliary contact with gold flash on the contacts for low signal level applications, shunt trip for AC 120-240 control voltages, and 48 inch leads.

CTA-ID : 2047488
Was this helpful?
What can we do to improve the information ?