Technical FAQs

Ask a Question

What is the replacement cover for a QO612L100DS, Series G1 or G3 load center?

Issue:
What is the replacement cover for a QO612L100DS, Series G1 or G3 load center?

Product Line:
QO Load Centers

Environment:
Indoor 100A Load Center

Resolution:
The cover with a door is part number - 4055345351.

NOTE: Labeling is not supplied on the replacement cover and the cost of the replacement cover may be close to, or exceed, the cost of a new device. You may want to consider buying a new device and use the new cover on the existing device.

CTA-ID : 2047228
Was this helpful?
What can we do to improve the information ?