Technical FAQs

Ask a Question

What is the wire range of the lugs provided in a CL10F kit?

The lug kit includes 6 lugs. Each lug will accept (1) #14 to #8 AWG solid copper conductor or (1) #14 to 1/0 AWG stranded copper conductor.


CTA-ID : 2046746
Was this helpful?
What can we do to improve the information ?