Technical FAQs

Ask a Question

What is the part number for the auxiliary switch for indication of HVL switch position? What is the contact rating of this switch?

The part number for the switch is 9007C62B2. The contacts are rated 10A continuous current for AC and 2.5A for DC voltages

CTA-ID : 2032327
Was this helpful?
What can we do to improve the information ?