Technical FAQs

Ask a Question

Do 8539 have to be de-rated due to altitude?

Yes. For example, at 4000` feet the thermal unit correction factor is x1.047, the current rating of the device is derated to 0.91x and the dielectric strength is derated to 0.92x.




CTA-ID : 2047290
Was this helpful?
What can we do to improve the information ?