Technical FAQs

Ask a Question

Is there provision for event counting in the MicroLogic trip unit of an SEF style breaker?

There are no provisions for event counting on the SE breaker Micrologic trip units. They can be tested using UTS-3 test kits, but there is no history of fault recording provision in the electronics of the trip unit.


CTA-ID : 2047282
Was this helpful?
What can we do to improve the information ?