Technical FAQs

Ask a Question

Can class 9013 pressure switches be used on a system containing a chemical called glycol (coolant)?

Issue:
Can class 9013 pressure switches be used on a system containing a chemical called glycol (coolant)?
Product Line:
Pressure switches

Environment:
9013 pressure swtches

Cause:
Can class 9013 pressure switches be used on a system containing a chemical called glycol (coolant)?
 
Resolution:
Yes. The 9013 diaphragms can be used on glycol systems.


CTA-ID : 2047104
Was this helpful?
What can we do to improve the information ?