Technical FAQs

Ask a Question

When ordering XB4 or XB5 LED light modules for the 22mm devices are the bulbs clear or the same color as the lens?

To the naked eye the LED will appear as clear. It is not a bulb it is a small chip that is embedded on a circuit board and has been coded for the proper color of the lens of the operator. The terminal markings, X1 and X2 and a small oblong will be printed next to the terminals in the color of the LED. A red LED will have these printed in red.


CTA-ID : 2047241
Was this helpful?
What can we do to improve the information ?