Technical FAQs

Ask a Question

How is a relay catalog number 8510XO20XTE1V02 converted from on delay to off delay?

The timing head mounts with two screws. It is removed and inverted or turned upside down to change the function of the timer from on delay to off delay. Refer to bulletin 30072-013-64 on Google for further instructions.


CTA-ID : 2047082
Was this helpful?
What can we do to improve the information ?