Technical FAQs

Ask a Question

What makes the QO120HID different than the QO120 breaker?

The QO HID breakers have proprietary construction features enabling them to pass UL testing and handle HID lighting loads. They are suitable for non-HID loads as well.


CTA-ID : 2047012
Was this helpful?
What can we do to improve the information ?