Technical FAQs

Ask a Question

Can a RU3040D400FL be used with an overhead service feed?

No, it cannot. The RU3040D400FL is a semi-flush mount device only, designed for underground feed. The Overhead Feed Trough, OCK400, is a surface mount device only, so it cannot be used in conjunction with the semi-flush mount CSED.

CTA-ID : 2046924
Was this helpful?
What can we do to improve the information ?