Technical FAQs

Ask a Question

Circuit breaker QGP22125TM has a listing on the label for 65K AIC at 240V and also one for 10K AIC single phase. Which one is correct?

This breaker is normally rated at 65K AIC, and the ``G`` character in the catalog number indicates this. The 10K AIC level is the rating for the breaker when used on grounded ``B`` phase applications, only.


CTA-ID : 2046897
Was this helpful?
What can we do to improve the information ?