Technical FAQs

Ask a Question

What is the suffix for the combination of the following suffixes for an LCL 3 pole type breaker?<br />8041 + 2100 + 1021 (copper lugs, bell alarm, and 120-240Vac shunt trip)

The suffix is a 2319.

CTA-ID : 2046789
Was this helpful?
What can we do to improve the information ?