Technical FAQs

Ask a Question

In a RC816F200CH generator panel application, can the back fed generator breaker be mounted into either positions 1 & 3 or 2 & 4?

The back fed generator breaker that would be used in conjunction with the RCGK2 generator kit will install in Positions 2 & 4 only.

CTA-ID : 2046906
Was this helpful?
What can we do to improve the information ?