Technical FAQs

Ask a Question

Are the Class 8736 Type S reversing starters available in NEMA 3R enclosures?

No, Square D does not currently offer the reversing starters in 3R enclosures, however the 4/4X enclosures are an option that could be used outdoors.


CTA-ID : 2047111
Was this helpful?
What can we do to improve the information ?