Technical FAQs

Ask a Question

What is the UL file number on the powerpact J frame breaker?

Issue:
UL File Number

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Cause:
UL File Number for job submittal

Resolution:
The UL number is E10027.

For additional information see catalog 0611CT1001 in our technical library.

http://static.schneider-electric.us/docs/Circuit%20Protection/Molded%20Case%20Circuit%20Breakers/0250%20A%20Frame%20PowerPact%20J/0611CT1001net.pdf

Technical Library:

http://products.schneider-electric.us/technical-library/


CTA-ID : 2046996
Was this helpful?
What can we do to improve the information ?