Technical FAQs

Ask a Question

What is the power consumption for the LC1F800 coil, LX4F8FW?

Product Line:

Tesys F line Contactors
This coil could be used directly with 110/120Vdc supply or with the rectifier, DR5TE4U, for 110/127Vac supply.
The Power consumptions are:
AC supply - The Inrush is 1700VA and the Sealed is 12VA
DC supply - The Inrush is 1900W and the Sealed is 12W

CTA-ID : 2046900
Was this helpful?
What can we do to improve the information ?