Technical FAQs

Ask a Question

On the instructions for the 9998PC337 it says to use a A65016-002-73 tool to install the o-ring. Is this still available.

No, we stoped making that part. It just assisted in installing that o-ring.
The same thing can be done with the cylinder of a ballpoint pen.

CTA-ID : 2047126
Was this helpful?
What can we do to improve the information ?