Technical FAQs

Ask a Question

Is there a multiple padlocking device available for a GV2 type manual starter? It is for Lockout/ Tagout purposes.

Yes. The catalog number is GV2V03. It will hold up to 6 padlocks with 6 mm shank size, maximum. Padlocks are not included.


CTA-ID : 2046703
Was this helpful?
What can we do to improve the information ?