Technical FAQs

Ask a Question

What is the cover mounting hardware/screws for the obsolete NH1B panels?

Issue:
What is the cover replacement mounting hardware/screws for the obsolete NH1B panelboard.

Product Line:
Obsolete NH1B panelboards.

Environment:
Obsolete NH1B panelboards sold and supported in the USA.

Cause:
Replacement hardware for the NH1B panelboard.

Resolution:
PK2TC, 26 inch wide panels only, is obsolete, no longer available. No other hardware is available.



 

 

 



CTA-ID : 2047009
Was this helpful?
What can we do to improve the information ?