Technical FAQs

Ask a Question

What is the wire range of the lug provided in a CL40F kit?

The lug kit includes 12 lugs total. Six of the lugs will accept (1) #1 AWG to 600 KCMIL copper conductors. Six of the lugs will accept (1) #6 AWG to 250 KCMIL copper conductors.


CTA-ID : 2046744
Was this helpful?
What can we do to improve the information ?