Technical FAQs

Ask a Question

What is the part number for the mounting screw provided with a PKOGTA4?

The mounting screw part number is 2142720241. A quantity of two are used to mount the ground bar.


CTA-ID : 2046742
Was this helpful?
What can we do to improve the information ?