Technical FAQs

Ask a Question

What is the part number for the mounting screws provided with a SN1200NA?

Issue:
Installation

Product Line:
Enclosed Breakers or Safety Switches

Environment:
Powerpact P or Heavy Duty

Cause:
Replacement 

Resolution:
The mounting screws are part number 21404-22201. A quantity of three are used.


CTA-ID : 2046741

Was this helpful?
What can we do to improve the information ?