Technical FAQs

Ask a Question

What is the part number for a 2 pole 30A breaker for Kohler load center QOPLILC?

QO230PLILC
Square D SQD QO230PLILC Specifications:
2 POLE; 120/240 VAC; 30 AMPERE; INTERRUPTING RATING 10000 AMPERE; LUG TERMINAL; WIRE SIZE 14 TO 2 AWG (ALUMINUM/COPPER); APPLICATION HID LIGHTING, HACR; PLUG ON MOUNTING; APPROVAL UL; USED ON POWERLINK[T] LIGHTING, CONTROL SYSTEM; POWERLINK[T] BRAND; QO MODEL


CTA-ID : 2046950
Was this helpful?
What can we do to improve the information ?