Technical FAQs

Ask a Question

What is the recommended torque for the line and load terminal screws on a 50 VA Control Transormer?

It is 20 lbs-in. (inch pounds) for the 8/32 screw.


CTA-ID : 2046839
Was this helpful?
What can we do to improve the information ?