Technical FAQs

Ask a Question

What is the hole diameter on the end where the roller would normally be attached for a 9007CA0?

The hole diameter is 3/16`` or 4 mm on the roller end of the limit switch lever arm.


CTA-ID : 2046825
Was this helpful?
What can we do to improve the information ?